2021-06-07 10:50 PM
Is there a way to send a single advertisement packet at a specific moment in code, ( without the mix/max interval time).
I want to disable advertisement.
And control it myself.
2021-06-08 6:44 AM
Could you explain the use case behind?
You can anyhow start the advertising phase with a max interval value and then wait for the “end of radio�? event (RF activity window ) and stop the advertising phase.
This way you have only one advertising window on the 3 channels 37,38 and 39.
2021-06-09 2:34 AM
Thanks for the answer.
The reason I am asking is that I would like to keep the same behavior from a previous controller.
Any chance a simpler possibility is available? A one shot? Instead of start stop?
2021-06-09 2:44 AM
Unfortunately not. We do not have any API enabling this one shot possibility.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.