2021-04-02 9:26 AM
Here is the function running in my STM32WB55CG:
/**
* this function can be nested
*/
void UTIL_SEQ_WaitEvt( UTIL_SEQ_bm_t evt_id_bm )
{
UTIL_SEQ_bm_t event_waited_id_backup;
UTIL_SEQ_bm_t current_task_id_bm;
/** store in local the current_task_id_bm as the global variable CurrentTaskIdx
* may be overwritten in case there are nested call of UTIL_SEQ_Run()
*/
current_task_id_bm = (1 << CurrentTaskIdx);
/** backup the event id that was currently waited */
event_waited_id_backup = EvtWaited;
EvtWaited = evt_id_bm;
/**
* wait for the new event
* note: that means that if the previous waited event occurs, it will not exit
* the while loop below.
* The system is waiting only for the last waited event.
* When it will go out, it will wait again fro the previous one.
* It case it occurs while waiting for the second one, the while loop will exit immediately
*/
while((EvtSet & EvtWaited) == 0)
{
UTIL_SEQ_EvtIdle(current_task_id_bm, EvtWaited);
}
EvtSet &= (~EvtWaited);
EvtWaited = event_waited_id_backup;
return;
}The code repeatedly calls UTIL_SEQ_EvtIdle(current_task_id_bm, EvtWaited).
current_task_id_bm is set to: CFG_TASK_SYSTEM_HCI_ASYNCH_EVT_ID
EvtWaited is set to: CFG_IDLEEVT_HCI_CMD_EVT_RSP_ID
Since I am not getting stuck there every time, it feels like some kind of race condition.
The comment seems to mention never leaving the while loop but I am not understanding it if it is telling me how to fix or prevent it.
Thanks for any help.
2021-04-02 2:36 PM
@Christophe Arnal, @Remi QUINTIN, these are serious bugs in a fundamental software component. Also, if the SEQUENCER is used in CPU2 firmware, these bugs could be even related to this serious issue:
2021-04-05 10:53 AM
void hci_cmd_resp_wait(uint32_t timeout)
{
UTIL_SEQ_WaitEvt(1 << CFG_IDLEEVT_HCI_CMD_EVT_RSP_ID);
return;
}I have also noticed that the function that calls UTIL_SEQ_WaitEvt is called with a timeout that is never used.
Is this something that should be implemented?
2021-04-06 12:41 AM
Hi Louis,
This problem generally happens when you are using wrong wireless stack for your application. For example if you want to use a ble application you have to update your stack to one of compitable ble stack to M0 core. Please search for wireless stack update for more. For addition if you are using one of st's example, there is a readme file thats tell you which wireless stack you have to use.
2021-04-06 6:23 AM
Thanks MeteHan, I am running a BLE application with the BLE Stack for the M0 core programmed per the release notes.
2021-04-06 10:55 AM
Hello,
Here are the feedback to the points raised :
Regards.
2021-04-06 10:59 AM
Hello,
This parameter is useless. It was introduced in the purpose of building a standard interface but in our STM32WB applications, it is not relevant.
Regards.
2021-04-06 11:21 AM
Hello,
This is a bit tricky. As long as you are in the startup phase, I believe it is unlikely that you are facing one of the race conditions that have been spotted and confirmed in the sequencer ( unless you added your own events in addition to the existing one).
To my understanding, you just received the system ready event from CPU2 and within the process that has received this system ready event, you sent some HCI command and for one of them, the CPU2 is not responding.
That would be goof if you could :
1/ confirm if you added or not your own events
2/ Identify which HCI command is not getting an answer from CPU2 - You may screenshot the function calling tree with your debugger.
3/ Check if this is the first HCI command that is not responded
4/ Check the value reported at the start of SRAM2 @0x20030000 where the CPU2 reports a keyword in case it has either detected an error or is in hardfault. Otherwise, you should read back that address of the shared table.
Regards.
2021-04-15 7:12 AM
Thanks Christophe.
I have not added any events. I will work to get you answers for you other questions.
Unfortunately with our hardware we did not leave ourselves any way to connect a debugger. I am working on code to read the value reported at the start of SRAM2 and print it out via UART. Is AN5185, Table 5, the best description of what we should expect to see?
One item of note that is a concern of ours is that this only seems to be happening with our latest batch of STM32WB55CGs. Previously, we have not seen this issue when running the same code but we are now seeing this happen on several units.
2021-04-19 3:09 AM
Hello,
As long as you have only traces over UART available, you may use the embedded HCI traces to check which command is pending.
This can be enabled in tl_dbg_conf.h
I would set following configuration
#define TL_SHCI_CMD_DBG_EN 1 /* Reports System commands sent to CPU2 and the command response */
#define TL_SHCI_CMD_DBG_RAW_EN 0 /* Reports raw data System commands sent to CPU2 and the command response */
#define TL_SHCI_EVT_DBG_EN 1 /* Reports System Asynchronous Events received from CPU2 */
#define TL_SHCI_EVT_DBG_RAW_EN 0 /* Reports raw data System Asynchronous Events received from CPU2 */
#define TL_HCI_CMD_DBG_EN 1 /* Reports BLE command sent to CPU2 and the command response */
#define TL_HCI_CMD_DBG_RAW_EN 0 /* Reports raw data BLE command sent to CPU2 and the command response */
#define TL_HCI_EVT_DBG_EN 1 /* Reports BLE Asynchronous Events received from CPU2 */
#define TL_HCI_EVT_DBG_RAW_EN 0 /* Reports raw data BLE Asynchronous Events received from CPU2 */
#define TL_MM_DBG_EN 0 /* Reports the informations of the buffer released to CPU2 */This should ouptut the system ready event received from CPU2 and all commands/events on either BLE or system channel exchanged between both CPUs.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.