2021-08-06 4:52 AM
How much flash memory is allocated for CPU2 flash and is it possible to write a RF firmware without involvement of CPU2
2021-08-06 7:06 AM
CPU2 is not designed to run user code. It is allocated the second half of the flash by default, although this is adjustable.
2021-08-06 7:23 AM
Hi,
Allocation depends on RF stack you choose. You can find RF firmware size on %HOMEPATH%\STM32Cube\Repository\STM32Cube_FW_WB_V1.12.1\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\
I think you can't use RF with CPU1 only.
2021-08-09 1:52 AM
what is the minium allocation which needs to be done for second core. I want CPU1 core to use the max flash
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.