NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
After an export then import (whether in "file system" or "archive file") of a working project, I cannot "build" this project agin after this export/import. While the basic project (before the export and the import i.e. the displacement) works perfect...
I am using the VBAT pin to measure the voltage of my battery, but the readings I am getting through this pin are always off by about 3%. The datasheet (https://www.st.com/resource/en/datasheet/stm32wle5cc.pdf#page=120) claims that there could be +-10...
ie, what drove the choice of PA12, specifically ?Using PA12 means that you have to power-up the VDD_USB domain - which, I think, adds some extra current consumption. See:https://community.st.com/s/question/0D53W00001Fncm7SAB/stm32l072-vddusb-supply-c...
Hi!Can someone help me to clear one moment in using LoRa.Let's say I have one RF remote control, which is pointed to 4-5 remote devices.How can my remote control distinguish replies from these 5 remote devices?Sorry if this is a dummy question. I'm n...
Hi guys. I am working on developing a product using STM32WB55RGV6TR. I referred to AN5042 and AN2867 to define the external crystal. Based on AN5042 if the used register setting for HSEGMC[2:0] is 0b111, the gm is 2.84mA/V. According to AN2867, the ...
Hi.I need to make a border router by combining stm32wb55 and raspberry pi. but i don't have any document associated this solution. in Thread_RCP example, as described below-----@par Application Description This application is used to demonstrate the ...
Good afternoon....I am new to STM and BLE. I have a while loop in main where I am checking conditional flags that could have been set in IRQs. All seems to work nicely. I then begin the process of implementing the BLE stack for peripheral. After ...
How do I find the real bluetooth address of a connected android device? I find the address in the mobile phone / tablet from the settings, but in the stm32wb55 program event HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE meta_evt->data structure, the address...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.