2021-12-16 7:06 AM
I am using the VBAT pin to measure the voltage of my battery, but the readings I am getting through this pin are always off by about 3%. The datasheet (https://www.st.com/resource/en/datasheet/stm32wle5cc.pdf#page=120) claims that there could be +-10% error on the ratio, this seems WAY too high to be at all useful so I was wondering if there was anyway to internal calibrate the resistors.
2021-12-16 8:05 AM
You would need to apply a known external reference voltage to VBAT and measure what you're getting to calculate the slope and calibrate.
This would need to be done on a per-part basis.
2021-12-16 8:46 AM
This was my fear, thank you!
2021-12-16 8:47 AM
> This would need to be done on a per-part basis.
I also wouldn't hold my breath relying on temperature stability of the divider.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.