STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 LPTIM PWM from LSE appears broken.

I am trying to get my STM32WB5MM-DK to output a PWM from LPTIM1 clocked from LSE in STOP mode.I created a fresh project with STM32SCUBEIDE selecting HSI clock for the main CPU and LSE clock for the LPTIM1.Then in User Code 2 section i put the followi...

JWieb by Associate III
  • 1730 Views
  • 2 replies
  • 0 kudos

STM32WL immediately wakes from shutdown sleep mode

I'm attempting to cause an STM32WL (currently on a WL55JC1 devboard) to sleep using the shutdown mode, and am running into a an issue where the MCU immediately exits sleep after it enters it.Here's what I believe to be the sleep related portions of m...

STM32WB55 Thread Stack not running on CP2?

I have been using the STM32WB55 Nucleo board successfully to run a CoAP server on OpenThread.I have designed a custom board which is very similar to the Nucleo board (same microcontroller).I successfully updated the FUS firmware following the Release...

0693W00000HoTz1QAF.png
YTalh.1 by Associate II
  • 1447 Views
  • 1 replies
  • 0 kudos

Resolved! Debugger VERY sensitive to shutting down??

I am using an STLINK-V3SET programmer / debugger. I connect to my target (STM32WB55) on a Midatronics Sharky Mkr board. I find that if I 'blink' or move funny the debugger after connecting shuts down and displays the following under the console win...

SWenn.1 by Senior III
  • 1405 Views
  • 1 replies
  • 0 kudos

Unable to successfully load BLE firmware because of FUS_IMAGE_NOT_AUTHENTIC so my code is failing in SHCI_C2_BLE_Init()

I have a custom board with an STM32WB55CEU (512K Flash) that is failing to start the BLE stack on CPU2 in the function SHCI_C2_BLE_Init(). I believe it's failing this function because it failed to load the BLE firmware (stm32wb5x_BLE_Stack_full_fw v1...

0693W00000HobzdQAB.png 0693W00000HocOsQAJ.png 0693W00000Hoc2DQAR.png
DPars.2 by Associate III
  • 2995 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.