STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB55 BLE How to set security modes.

I'm currently looking into how to actually set the security modes and security levels for a BLE device build on the STM32WB55RG chip.I have found the method to get what the security mode and level is:tBleStatus aci_gap_get_security_level( uint16_t Co...

AJoha.5 by Associate
  • 2128 Views
  • 2 replies
  • 0 kudos

STM32WL Geolocation

Does someone tried to have geolocation somehow with STM32WL Lora Stack?Supposedly it's included in the protocol using RSSI or TDOA against different gateways.Another way is to have direct link without gateway of known position nodes and the different...

DCama.1 by Associate
  • 1017 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL SUBGHZ Radio IRQ Lines

Hi there,I have a small question about the Radio IRQ lines on the STM32WL series. As far as I am aware, there are two MCU interrupts tied to the SUBGHZ radio: the RFBUSY interrupt (EXTI45) and the SUBGHZ_Radio_IRQ (EXTI44). However, when setting up t...

RLind.3 by Associate III
  • 3695 Views
  • 1 replies
  • 0 kudos

UART example for STM32WB55 "printf" prints gibberish. I see, the characters are sent to "HAL_UART_Transmit" are correct. BLE HRT example prints debug messages correct.

The printed message is:▒▒RT ▒▒▒n▒▒ E▒amp▒▒ ▒▒▒a▒g▒▒ ▒h▒ C ▒▒b▒a▒y p▒▒n▒▒ ▒un▒▒▒▒n ▒▒ ▒h▒ ▒▒RT▒Insteadprintf("UART Printf Example: retarget the C library printf function to the UART\n\r");

VadymS by Associate II
  • 910 Views
  • 1 replies
  • 0 kudos

Resolved! Conflict betwenn PKA and BLE after pairing.

Hello guys,I have a STM32WB application that runs bluetooth and PKA peripherals. We did setup this both peripherals a long time ago and was all going smooth. Our PKA is properly working using ISR, all the hardware semaphores were validated (including...

MBuen.1 by Senior
  • 1513 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.