2022-02-17 2:30 AM
I'm currently looking into how to actually set the security modes and security levels for a BLE device build on the STM32WB55RG chip.
I have found the method to get what the security mode and level is:
tBleStatus aci_gap_get_security_level( uint16_t Connection_Handle,
uint8_t* Security_Mode,
uint8_t* Security_Level );However I have not found a method or combination of methods to configure the actual security mode and level for my BLE chip.
Currently to setup the authentification requirements I'm using this method:
tBleStatus aci_gap_set_authentication_requirement( uint8_t Bonding_Mode,
uint8_t MITM_Mode,
uint8_t SC_Support,
uint8_t KeyPress_Notification_Support,
uint8_t Min_Encryption_Key_Size,
uint8_t Max_Encryption_Key_Size,
uint8_t Use_Fixed_Pin,
uint32_t Fixed_Pin,
uint8_t Identity_Address_Type );And I'm using the io capability method for that part:
tBleStatus aci_gap_set_io_capability( uint8_t IO_Capability );I can't find any documentation specifying how to actually configure the security modes and levels.
Security modes and levels are in reference to BLUETOOTH CORE SPECIFICATION Version 5.3 | Vol 3, Part C 5.2
Thankful for any insight on how to configure the security modes and levels, as well as enabling encryption.
Best Regards
2022-02-21 2:18 AM
Hello,
You can find information about security in programming manual PM0271, part 4.5 available here :
Online course on BLE security with STM32WB are also available on Youtube :
https://www.youtube.com/watch?v=YLgEBp7Ibu0&list=PLnMKNibPkDnGbiUxaLBqTdM2nNIVAk_MO&index=1
Best Regards
2022-02-21 6:15 AM
Thanks, I managed to resolve it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.