2022-02-09 11:35 PM
2022-02-10 12:01 AM
Did you tried STM32CubeMonitor-RF?
2022-02-11 3:30 AM
I don't think there is way to check the type of wireless stack once installed as it would be located in a secure protected area which is not accessible by the application.
I would like to correct my statement above.
There is indeed a way to get conformation data on the FW currently running on the M0+ core, calling the SHCI_GetWirelessFwInfo() command.
SHCI_GetWirelessFwInfo() command reads the informations relative to the loaded wireless binary.
A description of this command is available in AN5289 chapter 4.10 Device information table. Returned information is the Wireless firmware version, the Wireless Firmware Memory required by the wireless firmware and the Wireless firmware information.
Codes are listed in the shci.h file
2022-02-11 4:32 AM
Thanks. Is there (beside ReleaseNote.html) any application note that describes in detail characteristic and functionality of each firmware binaries and its API?
2022-02-11 4:59 AM
AN5270 is explaining the API used for all projects/stacks. they are of HCI or ACI levels.
2022-02-14 12:24 AM
Hello, what version of stack it should be used in BLE application?
UM2550 don't describe it clearly.
2022-02-14 12:44 AM
Version of WB FW package or type of stack?
For the version of the package, you should use the latest one that is located here
the latest one is v1.13.0 with a patch v1.13.1.
For the type of stack you should use for a BLE application, you can use stm32wb5x_BLE_Stack_full_fw.
stm32wb5x_BLE_Stack_light_fw is a light one with less features.
Other stacks are also provided depending of the system level you want to implement on the M4 core.
Please read the releases notes to get the description of each of them.
All the stacks are located under STM32Cube_FW_WB_VX.Y.Z\Projects\STM32WB_Copro_Wireless_Binaries
2022-02-14 2:39 AM
Yes, I asked of type of BLE firmware. Now I'm using the HCILayer_fw with stm32wb55VGY on Zephyr. And I would want to know that is there more appropriate firmware. And is there (over ReleaseNotes.html) some detailed description of characteristics of particular binaries of wireless stack for this MCU?
2022-02-14 9:06 AM
For the version available today, it is possible to use one the 2 stacks:
stm32wb5x_BLE_Stack_full_fw.bin
stm32wb5x_BLE_HCILayer_fw.bin => More appropriate as smaller
From version v1.13.2 onward, it is recommended to use one of the stacks listed below:
stm32wb5x_BLE_Stack_full_extended_fw.bin
stm32wb5x_BLE_HCILayer_fw.bin => More appropriate but no extended functions
stm32wb5x_BLE_HCILayer_extended_fw.bin => In case extended function are needed
2022-02-15 7:07 AM
What is the _extended_fw.bin ? I can't find it in STM32WB_Copro_Wireless_Binaries.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.