STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Achieving Lowest Power Mode with a persistent BLE Connection

I am working on a project where we would like a responsive and secure BLE connection to a battery powered sensor. If a supervisory timeout of 32 seconds is set, would the STM32WB be able to go into Standby while no data is needed to be sent and still...

Daniel L by Associate III
  • 2013 Views
  • 4 replies
  • 0 kudos

Downgrading BLE firmware

I have a WB55 with FUS 1.2.0 and I'm trying to use zephyr. However, zephyr is only tested up to v1.5 of the BLE firmware. I've tried everything from 1.5 to 1.13 and the lowest version I'm able to flash is 1.11. Is there a method to get to an older fi...

BGran.2 by Associate
  • 866 Views
  • 0 replies
  • 0 kudos

I-CUBE-LRWAN flash optimization

Hi,I need more 4kB of flash memory. Can I achieve this easily and safely by removing some not used functionality in the I-CUBE-LRWAN project?I suppose Lorawan Class B and C featues will not be needed. Can I just exclude this files from the project an...

Marcuka by Associate III
  • 956 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB Fails on SHCI_C2_BLE_Init

Hello! I'm working with a custom STM32WB10CCU board and can't seem to get BLE working.Here are the details:I have no LSE on the board.. just HSE. I'm configuring RFWKP to HSE/1024 and RTC to HSE/32 (I know that LSE is strongly recommended -.. but fro...

WSH by Associate III
  • 6263 Views
  • 9 replies
  • 1 kudos

Recommended TCXO for STM32WL Design

We design a new product where we use STM32WL microcontroller and in the datasheet ST is recommended to use NT2016SF-32M-END5875A, it was not in stock everywhere. We planned to use the ECS-TXO-20CSMV-320-EY-TR TCXO in our design. Please share your rec...

HVeer.1 by Associate II
  • 1728 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.