NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi everyone,I'm developing a device based on a STM32WB55 which has a USB interface. Using CubeMX I created a project with a Custom HID device, FreeRTOS + CMSIS v2.I need to send frames of a proprietary protocol which content usually don't exceed 64 b...
@file stm32wbxx_hal_qspi.hQSPI_CommandTypeDef -> DdrHoldHalfCycle#define QSPI_DDR_HHC_ANALOG_DELAY#define QSPI_DDR_HHC_HALF_CLK_DELAY ((uint32_t)QUADSPI_CCR_DHHC)
Hello,I'm trying to set up my WB55 USB Dongle to act as an iBeacon device. Following documentation on how to use USB dongle I flashed TransparentmodeVCP binary file on my board and have successfully connected to it with Cube-RF software.I set up beac...
Dear Community,I'm using a P-NUCLEO-WB55 Board and Dongle, until now only with ST examples.I'm trying to perform firmware update using BLE OTA (switching from BLE_HeartRate_ota to BLE_p2pServer_ota for example) and am facing a problem.The same proble...
Hi. I am Jay working with STM32 ST board (MB1355C and USB dongle) to build Zigbee application. To become familiar with STM32Cube Firmware, I picked and ran one example of STM32Cube_FW located at STM32Cube_FW_WB_V1.13.0\Projects\P-NUCLEO-WB55.Nucleo\A...
I've hit the limit of my research and don't have any experience writing to flash other than at compile time using the keyword 'const', but that doesn't help me because I need to be able to continuously write data. I have a very basic and general sens...
HI all,I’d like to create a system communication using LoRa protocol between 2 devices, I don’t want to use TTN. I’m newbie with LoRa I’ve seen Seed provide SDK to use LoRaWAN but I don’t want to use gateway or server. To be simple I have one device ...
So, I have TIM2 setup to trigger an ADC conversion and the DMA moves the samples out to RAM. I want to do this every 100us for 1000 iterations. Sounds pretty straight forward. There are 3 ADC channels being sampled using the sequencer on every tri...
Hi all,I've been trying to use the STM32WB55 Dev Kit and if I generate the project with the peramitirs below and then try to build the project I get this error;*** Error Code *** C:/Users/bryce/STM32CubeIDE/workspace_1.3.0/STM32WB55-MB1355C/Debug/....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.