STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB & SPP

Hello Everyone,Intro. Our embedded project was defined based on the BC127 Bluetooth module, which enjoyed Melody 7.0 firmware. We used the SPP protocol in such a way that a new virtual comport is added to my device manager list when the operating sys...

ptagh.1 by Associate II
  • 1982 Views
  • 1 replies
  • 0 kudos

Resolved! How do I get the application for hands on workshop?

Hi Im looking for he hands on application for the "mooc - stm32wl workshop - 4 point" as on you tube https://www.youtube.com/watch?v=n7OoTStkczs . Anyone got a link to where I can get the exact same applications?Many ThanksScott

Resolved! Nucleo JC1 LoRaWAN Dual Core example doesn't compile.

arm-none-eabi-gcc -o "LoRaWAN_End_Node_DualCore_CM0PLUS.elf" @"objects.list" -mcpu=cortex-m0plus -T"/Users/ben.blouin/dev/LoRaWAN_End_Node_DualCore/STM32CubeIDE/CM0PLUS/STM32WL55JCIX_FLASH.ld" --specs=nosys.specs -Wl,-Map="LoRaWAN_End_Node_DualCore...

bblouin by Associate III
  • 1521 Views
  • 3 replies
  • 0 kudos

Where to find Lora header in packet?

Hi Im using the SUBGHz in Lora mode for communication with point to point. What I want to do is design low power communication. I plan to send the first packets from the battery node to SF12 , then the permenant connection node will detect the sign...

Resolved! Trace Synchronization Error on NUCLEO Board

I am currently using NUCLEO-WL55JC board. However, I could not initialize the logic analyzer.The watch tab works well, but the analyzer window seems not working. And, I have an error at the bottom showing "Trace: No Synchronization". I set the core f...

0693W00000LyFetQAF.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.