NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm trying to understand how I program the BLE Stack and FUS in the CPU2 of STM32WB55G (1Mb). When I use the binary available of ST repositoy, in default mode I program the "stm32wb5x_BLE_Stack_full_fw.bin" in address started 0x08000000, but in the r...
Hello,I want connect to a bluetooth device/sensor from stm32wb and configure the device : for example confgure the period that it shoold advertise for.Is that possible? If yes how ?
I'm using SAI PDM interface to record pdm audio coming from 4 microphones. I'm using a stm32wb55rg and the memsmic1's example.There are some parts I don't understand with the SAI configuration in the example. Here is a part of the code provided in th...
I have a question about how to correctly update a value of characteristic of custom BLE service on STM32WB50CG. The project was set up with CubeMX following their official tutorial: https://www.youtube.com/watch?v=i10X4Blr8ns.My main application is r...
Situation - I'm combining code examples from the STM32WB Opus Library code, with that of the Echo Cancellation (AEC) Function Pack. Using the code base to have support for a microphone, speaker, and Bluetooth. When implementing the code for the CCA01...
HiI'm using Nucleo-WL55JC1 STM32WL development board for LoRaWAN end node dual core and i have a custom board with MCU STM32WLE5CBU6 for LoRaWAN end node single core.I have configured LoRaWAN end node protocol parameters like this documentation (http...
We are also facing same tx timeout in our custom designed hardware. We are using XO clock in the design and donot have option for TCXO. Please share your inputs whether STM32WL55JC1 will work with XO clock. We got struck with TX Timoeut issue.
Hi, I am using an STM32WB50 and i need to find a way to discover fus and stack versions installed not using an external tool but directly by reading some register or using specific function. Is there a way to do this?Thanks
Hi...Community Hope you all are doing well Recently, I'm dealing with the STM32WB custom hardware In my application, i need the USB VCP logs during the BLE operation And that's how I'm using USB CDC for the communication with the serial terminal For ...
We dont require any of the RF features in our use case. Had to choose this MCU due to chip shortage. Just want a functionality of a regular STM.Can we just use application core independently ?Is it possible to disable RF (Bluetooth radio ) completely...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.