2022-05-06 2:14 AM
As I said, I get the assertion "zigbee_app_info.colorControl_server_2 != NULL" failed error from a standard debug function in the code.
I thought it could have something to do with this struct, which is a bit above it.
struct ZbColorClusterConfig colorServerConfig_2 = {
.callbacks = ColorServerCallbacks_2,
.capabilities = ZCL_COLOR_CAP_HS,
}I feel like it has to be something I have to add here because this struct is checked to be NULL, but I can't seem to find what it is I have to add.
The place where the struct is set to something other than NULL is here:
zigbee_app_info.colorControl_server_2 = ZbZclColorServerAlloc(zigbee_app_info.zb, SW2_ENDPOINT, zigbee_app_info.onOff_server_2, NULL, 0, &colorServerConfig_2, NULL);From what I could gather, this would allocate the space needed, but I guess something goes wrong and no memory is allocated.
This error occurs every time I start a new project and add the color control cluster. So it happens even when I haven't added anything.
Solved! Go to Solution.
2022-05-10 12:24 AM
So If anyone is also like me stuck here, the problem was the capabilities.
The code for it should be:
.capabilities = ZCL_COLOR_CAP_XY,This is the only way I found to get it working, I don't know what the other capabilities are for.
At least I solved it : )
2022-05-10 12:24 AM
So If anyone is also like me stuck here, the problem was the capabilities.
The code for it should be:
.capabilities = ZCL_COLOR_CAP_XY,This is the only way I found to get it working, I don't know what the other capabilities are for.
At least I solved it : )
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.