NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
In my condition, I have to use the AU915 frequencies due to the rules of my localization. So, I changed the frequency in the compiler and in the firmware I updated the connection mode to ABP, because I've been working with LoRa and for me always work...
I want to build USB-BLE bridge using nucleo board - something like virtual serial connection between boards. I want to connect both boards using Bluetooth interface. Then USB dongle should forward data from USB CDC to Nucleo board and vice-versa fro...
Hi,I finally got my zigbee up and running on v.13.xx but it stops working, properly in M0 core after 5-20seconds.However I thought it would be good to go to 14.1, so i did, made a project.But i cannot compile the project.It is based on Cube...I get t...
Hi all,I'm on a P-NUCLEO-WB55 Nucleo Board (MB1355C) and I'm trying to connect an example to a Windows (Win10) PC via BLE.I'm using the latest firmware version STM32Cube_FW_WB_V1.13.2 and flashed the Copro Wireless binary stm32wb5x_BLE_Stack_full_fw....
Hi, I'm using a couple of functions: tBleStatus aci_gap_additional_beacon_start(...);and tBleStatus aci_gap_additional_beacon_stop();The point is that aci_gap_additional_beacon_stop() periodically returns error code 0x0C, which means "command disallo...
Hi,I'm struggling to add low-power features to my device application, hopefully I can get some help here.What do I want?My device is sampling sensor data (52Hz) and saving it periodically to external flash memory. When the device is running in sampli...
Hello everyone,I am currently working on the hardware design of a STM32WB55 and there is an information I would like to clarify.In the AN5165, it is explained that the RF track should be matched at 50 ohms. However, on page 43/48 - figure 36, there i...
I'm developing an STM32WB55 microcontroller but I'm straggling with programming.I want to control the microcontroller using its BLE module but there is no good programming example. So, is there any recommendable example to write the memory of the mic...
Hello,I just had some custom boards with STM32WB55RG and I would like to flash the BLE stack into the microcontroller.Files I'm trying to install on the device:stm32wb5x_FUS_fw.bin(v1_0_2)stm32wb5x_BLE_Stack_full_fw(v1_13_3)and firmware fileBut devic...
Hello,We are running STM32WB RTC block from LSE.Usually it works as expected (hours at a time).One in a while, the RTC->SSR resister jumps back (up as it is a countdown reg) couple of ticks (~100 ticks) and continues from the same point as normal.It ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.