NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have STM32WB55 nucleo pack.The installation of STM32CubeProgrammer brought two tools STM32MP_KeyGen_CLI.exeSTM32MP_SigningTool_CLI.exe. Following instruction https://wiki.st.com/stm32mpu/wiki/Signing_tool, a sample of signing command:./STM32MP_Sign...
Is STM32WB55REV6 has Trusted platform module (TPM) either integrated in to the microcontroller..? or additional module to enable the device level security (TBD).Can you please help me on the ablove
I need a 32-channel ADC system but my target microcontroller(STM32WB55) only has a 16-channel.So, I want to design two microcontroller systems but the timing would be the biggest problem.So, I wonder what's the best way to build a dual microcontrolle...
Hello,I wonder how the STM32WB device should be entered in SLEEP or STOP mode. Any specific actions to reduce the total consumption to the minimum, particularly thinking to the radio? When is it good to enter SLEEP or STOP mode ?If anyone can point a...
Hi All,I am trying to connect my p-Nucleo-wb55 board to a joystick using Bluetooth.the joystick I am working on is DualShock 4, and I have obtained its address from my PC.So is it possible to make a connection with the MCU with just the Bluetooth add...
Hi... There Hope you all are doing well For the past few days, I'm dealing with the LoRaWAN Firmware having class-CIn my application, I need the continuous connection between Node to gateway and gateway to the Network server (As I want to receive the...
Hi,I wrote an application for the BME680 sensor on the LoRa-e5 (based on STM32WLE5JC).At the begin everything works normal but after about 70 minutes no more messages come to uart.in the Error Log I got this message:eclipse.buildId=Version 1.10.1 jav...
MCU: STM32WLE5CCIDE: Stm32CubeIDE 1.9.0I have generated a project using MX and thought I'd try the generated function for reading the temperature SYS_GetTemperatureLevel().It seemed to output rubbish so I started digging.SYS_GetTemperatureLevel() cal...
Hi, I have shared my project schematic. it's should work or not? (SMPs not used)Problem : BLE cannot advertise, but this configuration in STM32CubeIDE can work with NUCLEO-WB55.
I'm using the STM32WLE5JBI6 part which has 128kB Flash and 48kB SRAM but it is not clear what address these have as the STM32CubeMX generated linker and header files is for the 256kB Flash and 64kB SRAM partAm I correct in thinking the layout for thi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.