2022-08-14 3:41 PM
Hi,
I'm using a couple of functions:
tBleStatus aci_gap_additional_beacon_start(...);and
tBleStatus aci_gap_additional_beacon_stop();The point is that aci_gap_additional_beacon_stop() periodically returns error code 0x0C, which means "command disallowed".
NOTE: I'm using STOP2 mode, if I comment out this part (not allow MCU enter sleep mode) the aforementioned function returns 0x00 all the time.
How to use STOP2 mode in a proper way?
2022-08-17 10:08 AM
Hello,
In order to see how to use STOP2 mode, you can look BLE_HeartRate example which allow to do STOP2 low power mode using low power manager.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.