STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! Lora config at 433MHz

Hello,I used a GFSK configuration with 433MHz and it is work very well,I try now to migrate to Lora modulation. i used a basic config, but the receiver on the other side receive less then 1% of sent frames ! (even transmitter and receiver are very cl...

0693W00000QO4S1QAL.png 0693W00000QO4T4QAL.png
malarab by Senior II
  • 3654 Views
  • 6 replies
  • 0 kudos

STM32WB15CC allow CPU1 to access all resources

I am trying use the stm32wb15cc to run an application on CPU1, but with no application in CPU. I don't need the RF side at all and want to hold CPU2 in reset and allow CPU1 to access all the Flash and Ram.However this does not seem possible as Option...

ALest by Associate II
  • 3990 Views
  • 10 replies
  • 1 kudos

LoRa WL55 workshop videos?

I attended the Tuesday Sept 7th session of the lorawan-with-stm32wl-soc-workshop-ame-2021 I was unable to complete the workshop during the allotted time.  I would like to complete the training. Are the videos available?

Use of STM32CubeIDE with LoRaWAN_End_Node: create a project.

I'm working with STM32CubeWL, version 1.1.0. Starting a new project from .ioc file seems that the firmware will be upgraded to the version 1.2.0. Is this correct? Can I find, somewhere in the source code, the firmware version?Can I avoid this behavio...

0693W00000Su0mEQAR.png
FRest.1 by Associate III
  • 3601 Views
  • 5 replies
  • 0 kudos

Resolved! How to install STM32CubeWB from STM32CubeMX

HiI am trying to install STM32CubeWB from STM32CubeMX by following YouTube "STM32WB Getting Started Series: Part 3, Tools Install". After clicking "INSTALL/REMOVER" button, I got message "The Updater is already in use and checking the server. Please ...

NWang.2 by Associate II
  • 1678 Views
  • 1 replies
  • 0 kudos

STM32WB5M BLE MESH LIBRARY can not find unprovisioned device

I am trying to build an embedded provisioner for the stm32wb5m, but i am not able to find an unprovisioned device.I am using the example "BLE_MeshLightingProvisioner" for the WB55 nucleo Board as reference.The Initialization of the STM32WB and the co...

CBuch.1 by Associate III
  • 1458 Views
  • 1 replies
  • 0 kudos

Resolved! WHY PER CALCULATION DOES NOT WORK AS EXEPTED?

Hi, following your DS, LoRa PER = 1%. While RF examination, for BW= 125KHz and SF=7, the sensitivity of the micro controller is around -125dBm for PER = 1%. When we change the value of SF to 12, the sensitivity should change to -138dBm but in reali...

TLit.1 by Associate
  • 2039 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.