2022-08-29 1:20 AM
Hi, following your DS, LoRa PER = 1%. While RF examination, for BW= 125KHz and SF=7, the sensitivity of the micro controller is around -125dBm for PER = 1%. When we change the value of SF to 12, the sensitivity should change to -138dBm but in reality we get sensitivity around -110dBm for PER = 1%. In -138dBm we have got Per of ~20%.
Our PER calculation has taken from your lib : Subghz_Phy_Per.
Our code is attached.
I would like to get a feedback from you why it is not working.
Thanks,
Tamar
Solved! Go to Solution.
2022-08-29 6:24 AM
Expected?
The math presumably isn't the problem, but rather the counts that drive the computation.
Bunch of TESE_MODE references that should be TEST_MODE
In continuous mode there shouldn't be timeouts, so everything is errors.
Check the raw error counts, and address those.
Don't block in the process, if your want periodic output base it on tick counts not delays
2022-08-29 6:24 AM
Expected?
The math presumably isn't the problem, but rather the counts that drive the computation.
Bunch of TESE_MODE references that should be TEST_MODE
In continuous mode there shouldn't be timeouts, so everything is errors.
Check the raw error counts, and address those.
Don't block in the process, if your want periodic output base it on tick counts not delays
2022-08-30 12:55 AM
Thank you very much!
Right that was the problem..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.