STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

No St Link Detected STM32WL55JC2

Hello, I recently bought an STM32WL55JC2 board (nucleo). I have downloaded the STM32 IDE.When I connect the card in USB directly to my pc there are three LEDS that blink successively (red green blue).I can build my project (empty) on STM32IDE on both...

0693W00000Uoei8QAB.jpg 0693W00000UoehyQAB.jpg
BNamu.1 by Associate II
  • 4574 Views
  • 13 replies
  • 0 kudos

Resolved! What is the switching speed of a GPIO pin for STM32WB55?

I want to use an external multiplexer to increase the number of ADC but switching speed is one of concern.Fortunately, some multiplexer has a 13 ns switching speed (~100 MHz) and I'm planning to switch it using a GPIO signal.However, it arises concer...

KKIM.6 by Senior II
  • 2056 Views
  • 3 replies
  • 0 kudos

STM32WB

I use my own board (as ble server) to notify the client, each notification is 120 bytes, I found that I can only transmit 30 per second. Actually my requirement is 100 transfers per second.Do I need to modify anything?

Lep by Senior
  • 1668 Views
  • 4 replies
  • 0 kudos

I want to control a remote controlled car, could you advise me what is best to use? I had thought about the 5G that is present in my city but I don't know if it is a good idea. I would also need to receive the audio and video signal

 I had thought about the 5G that is present in my city but I don't know if it is a good idea. I would also need to receive the audio and video signal. is it possible to make?

Alfred04 by Associate
  • 718 Views
  • 0 replies
  • 0 kudos

Unknown aci_gatt_proc_complete_event

I am getting this event upon sending : ACI_GATT_EXCHANGE_CONFIGI can't understand why I am getting it. What procedure is complete?According to AN5270 I should not get it for that command.

0693W00000VOBljQAH.png
DS.4 by Senior II
  • 1119 Views
  • 1 replies
  • 0 kudos

GPIOB not enabled on STM32WL55JC2

Hello, I just received my WL55JC2 card and I would like to blink one of the leds on the card with a very simple line of code but I don't understand why it doesn't work. I noticed that the led was pinned on the GPIOB which was not enabled in the gener...

0693W00000VO8rjQAD.jpg 0693W00000VO8roQAD.jpg 0693W00000VO8rtQAD.jpg 0693W00000VO8s8QAD.jpg
BNamu.1 by Associate II
  • 1106 Views
  • 1 replies
  • 0 kudos

Resolved! Over the air (OTA) firmware update for STM32WLE5xx MCUs

Hello,The datasheet for STM32WLE5xx states, that this series is capable of OTA firmware update, however I am not able to find any resources on how do perform it. The only document that shows up is the AN5554 application note on firmware update over t...

MLisa.1 by Associate
  • 2088 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.