STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! How can I reset ADC measurement for the next measurement?

Right now, I'm focusing on increasing ADC channel.I assembled the STM32WB55VG microcontroller and 8:1 mux.The mux is contolled by three GPIO pin for [2:0] encoding to select channel.The output of mux is connected to the ADC and I can see the ADC data...

KKIM.6 by Senior II
  • 2441 Views
  • 2 replies
  • 0 kudos

STM32WB55RB can't allocate memory after GPIO Interrupt

The problem can be simplyfied to this code:int startFlag = 0;void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin){ startFlag = 1;}int main(){ if(startFlag== 1){ //crashes at first iteration (Hard_Fault_Handler) int *test = malloc(sizeof(i...

PSpin.2 by Associate
  • 1523 Views
  • 2 replies
  • 0 kudos

Stack BLE random crash on STM32WB

I have an STM32WB that is configured in central, it connects to 8 devices in peripherals mode at the same time. This configuration works well, but from time to time the BLE stack does not respond, I see 8 peripherals disconnected and I do not receive...

JSalv.1 by Associate
  • 1104 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.