2022-08-29 7:48 AM
I want to use an external multiplexer to increase the number of ADC but switching speed is one of concern.
Fortunately, some multiplexer has a 13 ns switching speed (~100 MHz) and I'm planning to switch it using a GPIO signal.
However, it arises concerned on the switching speed of the GPIO pin also.
What is the switching speed of a GPIO pin for STM32WB55 microcontroller?
Solved! Go to Solution.
2022-08-29 9:23 AM
i know, it is hard work - but , if you would RTFM ,
you could read it yourself, on P. 137 : 1,7ns.
2022-08-29 8:57 AM
How do you plan to control that pin, exactly?
The ADC has a sampling phase and then a conversion phase. You can switch anytime during the conversion phase. Switching speed is surely not a concern at all.
Read the ADC chapter in RM.
JW
2022-08-29 9:23 AM
i know, it is hard work - but , if you would RTFM ,
you could read it yourself, on P. 137 : 1,7ns.
2022-10-27 1:02 PM
Right now, I'm focusing on this issue.
I assembled the STM32WB55VG microcontroller and 8:1 mux.
The mux is contolled by three GPIO pin for [2:0] encoding to select channel.
The output of mux is connected to the ADC and I can see the ADC data using DMA.
If I select one channel in the mux, I can collect data exactly.
However, if I operate the mux with switching channel (I gave ~1 ms of interval for each channel), the most recent channel data is filled to the previous channel (last channel data only appears in all the channel data).
I know that the microcontroller has single ADC and multiple channel itself and it works very well when I use scan conversion mode. It imply that there is a very quick reset state in the ADC to restart measurement for next channel.
So, I wonder how can I force to reset ADC measurement in the coding.
Is it possible?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.