STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Flash Operations Initializations.

Hi Team,We are using the STM32WB55 Series for our project. We are using specific flash sectors (8) for our config data. Is there any specific Initializations are required for Flash Operations which is similar to other peripherals like Clock, UART, I2...

STM32WB55 Comparator max speed

I have a board NUCLEO-WB55 and I'm testing some examples.I'd like acquire a sine wave about 14 MHz and convert to square wave with internal comparator. I can't find enough informations on datasheet if it's fast to acquire this signal.Thank you for su...

juvann by Associate III
  • 1151 Views
  • 1 replies
  • 1 kudos

How to disable any kind of polling in SED devices?

Dear all,I am happy playing with STM32WB kits but there is something that really annoys me.I am creating a very low power temperature sensor configured as SED. The problem is after every payload I send it stays in fast polling every 500 ms for some t...

SFern.21 by Associate
  • 1072 Views
  • 0 replies
  • 0 kudos

Resolved! Using commands, how to "run after programming" ?

Hello, To push code using commands, i use this : STM32_Programmer_CLI.exe --connect port=SWD mode=UR reset=HWrst -d file.elfBut I would like the program to run after the programming step is complete (same behaviour as when programmed with STM32CubePr...

LVolp.2 by Associate II
  • 5891 Views
  • 2 replies
  • 2 kudos

Questions to ST wireless chips

Hi!We want to build a localization system based on AoA, which should localize BLE-Beacons. Therefore, I have a few questions to the ST BLE-chips:1. Is it possible to configure a device from the product portfolio to a fixed radio channel, on which BLE...

MHehn.1 by Associate
  • 1249 Views
  • 1 replies
  • 0 kudos

Programm NUCLEO-WL55JC with external STLink

Hi,I have a NUCLEO-WL55JC (revision 0E) that stop working after I flashed the LoRaWAN_End_Node example project. With the CubeProgrammer, sometimes I can manage to update the STLink Firmware (if I keep rebooting the board), but I can't ever connect to...

A Pica by Associate II
  • 2461 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.