STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Does there exist an STM32WB5MMG reference manual?

I am aware there is a datasheet, but it does not contain the info I need. I am trying to configure timer triggered timers for my project, so I would like to know the internal trigger mapping for each timer. I am hoping to find something similar to th...

0693W00000WKIe7QAH.png
Lloyd44 by Associate
  • 1882 Views
  • 2 replies
  • 0 kudos

Simultaneous BLE connections on WB55

Hi, I'm using the STM32WB55 as a BLE peripheral. The goal is to support multiple simultaneous connections with different Centrals, so that the peripheral can broadcast its characteristics to multiple clients.To accomplish that, my code re-enables adv...

Akos P by Associate II
  • 7936 Views
  • 13 replies
  • 1 kudos

Resolved! Need info on optimal Set_PaConfig

Reference manual RM0453 and AN5457 - Rev 2 give some info on optimal PA and TxParm settings but the data is incomplete and appears to be inconstant. For example, Table 2 of AN5457 says for RFO_HP, +14dBm set paDutyCycle to 0x2 and TxParms to 14. The ...

MPend.3 by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos

RFM95W on STM32G070

Hi,I have a problem on the LoRa transmission.If I use STM32F103 on SPI 1, LoRa transmission works.And if I use the STM32G070 with the same code the LoRa transmission doesn't work.What is the différence on the SPI in the STM32G070 ?

ttim.2 by Associate
  • 2327 Views
  • 2 replies
  • 0 kudos

Messy UART message

I'm trying to logging Teseo LIV3FL using my STM32 Nucleo-WL55JC1. I've tried in my ESP32 before and it works as it is. However, when I tried to use them in my Nucleo board, the message are messy or mixed between other messages. Expected Output:Receiv...

0693W00000WK4VVQA1.png
AFidi.1 by Associate II
  • 1287 Views
  • 2 replies
  • 0 kudos

example for STM32WL55 without the sequencer?

Is there a simple example for STM32WL55 that does not use the sequencer?I want to integrate the LoRa radio with my code and my own task scheduler.From CubeMX, the SUBGHZ module works well but when I add SUBGHZPhy, everything seems to break.

GHaid.1 by Associate
  • 1630 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.