2022-12-10 6:39 AM
Dear all,
I am happy playing with STM32WB kits but there is something that really annoys me.
I am creating a very low power temperature sensor configured as SED. The problem is after every payload I send it stays in fast polling every 500 ms for some time. This drains the battery. As it is only a temperature sensor I never expect to receive commands so I do not need any kind of polling. How can I permanently disable it?
Update:
Looks like Zigbee_OnOff_Client_SED works as intended using anothe STM32WB as coordinator. Power consumption in stop2 is as expected around 3uA.
If I use another device such as zigbee2mqtt or xiaomi gateway it has a different behaviour. After sending a command it generates 6 poll requests and after that CPU2 is not going to STOP2consuming 1.8mA.
The point is that right after transmitting it goes into stop2 but around 1 second after it wakes up and stays up until next transmission.
Is there any way to avoid waking up too early?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.