NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear All,I have managed to get the LoRaWAN_end_Node_DualCoreFreeRTOS sample working and now I am trying to get this sample to perform a continuous wave.I know that I need to use the mailbox system in order to send the proper settings and commands, bu...
Hi,I want to know the difference between EXTI PR1 and EXTI PR2 registers in stm32wb55xx.
We are using an STM32WL55 (NUCLEO-WL55JC2) and don't understand RCC_BDCR_RTCEN. Our system is configured to be woken up from Stop 1 Mode via RTC wake-up, clocked by LSE. This works, but we wonder about a detail.According to RM0453, RCC_BDCR_RTCEN is ...
Hello,I am currently using STM32WB55 with QSPI external flash.Currently, the plan is to use it without Bluetooth, for now.I am able to write and read the flash in the program.The plan:Record for 24 hours with DMA from sensors to flash.Upload another ...
STM32u585I and STM32WB5MMI'm struggling programming the bluetooth module of the U585I board.Stlink is connected in CN5, board is powered with CN8, but how to program the stm32wb (the Bluetooth module).With the CubeProgrammer, I can connect only to th...
The stm32wb55 writes data to the sd card in real time through FATFS, and the function f_write() will take tens of ms. I want to use two buffers, one buffer to store data, and one buffer to write data to and from the sd card (can this avoid the delay ...
I have a custom board running the STM32WB55. My medium term goal is to use BLE to perform OTA updates for my firmware. I'm trying to leverage the BLE_p2pServer BLE_p2pServer_ota examples from the as a starting point, but I'm getting stuck at one o...
Hello, I have a STM32WLE5JB, and a want to wakeup the chip from sleep mode to have multiple task. (Read a sensor every x sec) externally from the RTC that is tied to the lora TX delay.So i have the code that include the lora stack without any modific...
On STM32WL is the rfbusys only available in polling mode or is there an interrupt linked to it ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.