STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How to use timer interrupt to trigger the sending of BLE data every specified second for STM32WB5MMG using STM32CubeIDE?

Hi,I'm using STM32WB5MMG and want to send 8-bit data through BLE every specified duration (e.g. 1s). I have tested the Bluetooth and timer interrupt separately and both works fine. However, when I tried to trigger the Bluetooth using timer interrupt ...

0693W00000YAOY8QAP.png 0693W00000YAX34QAH.png
SWong.10 by Associate II
  • 7588 Views
  • 8 replies
  • 1 kudos

I have designed a STM32WL55JC2 board with reference to en.MB1389-WL55JC-lowband-D04_Schematic and got it manufactured. Now When i try to program the chip with STM32CubeIde version 1.11.2, the following error occurs.

Log output file:  C:\Users\ASHSIR\AppData\Local\Temp\STM32CubeProgrammer_a10808.logST-Link Server is running on port : 7184ST-LINK SN : 3A2C0A0011145243574D4E00ST-LINK FW : V2J37S7Board    : --Voltage   : 3.18VSWD freq  : 4000 KHzConnect mode: Under ...

scora.1 by Associate
  • 2115 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB55 RCP evaluation

Hi,My 1st post here, so please forgive me if I'm posting this in the wrong category.2nd disclaimer, I'm predominantly a HW engineer, so I have a limited amount to SW experience.I've been trying to put together a OT border router application on a Beag...

romihs by Associate II
  • 1525 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLE5 high current consumption in Stop2 (RAK3172-SIP)

HelloI am trying to implement low power mode with STM32WLE5 MCU (as a part of RAK3172-SIP).However, the current consumption is unreasonably high.I measure around 200uA with 3.6V and around 150uA with 3.3V.Did many tests with different configurations,...

YDOVG.11 by Associate II
  • 2381 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.