NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi guys,Do you ever had a thought about making the CoPro firmware opensource and allow the community to participate the development? I see that the progress in maintining the Thread protocol is quite slow compared to the Openthread main repos, also s...
Hi I'm trying to create a new project from an .ioc file and I get 2 errors, first the "code generation could not be done most probably because the neccessary firmware package is missing, not able to complete stm32Cube project creation" then as sugges...
I am writing a driver for the STM32 to get the data from the front-end board, AD5940 using the SPI communication. I am using the AD5940 library available at the : https://github.com/analogdevicesinc/ad5940lib.STM32WB55xx has been used. I have configu...
In my application, I receive a message from LoRa and intend to transmit it via UART1 which is set to PA9 and PA10. However, when I check the UART RX using a logic analyzer, I do not receive anything.I have tested the UART1 alone in a simple project, ...
Some of our devices stopped working properly. We can see an advertisement, however the advertisement does not contain a device name. Furthermore, it is not possible to connect to the device. The interesting part is, that the device seems to be broken...
If server1 is connected to the client and when I try to connect with server2, will server1 still be connected?because once 2 servers are connected I am not able to GATT Write attribute to an individual server.I am able to write only newly connected s...
I want to get data from Bluetooth module to main MCU via Rx Tx (Like HC-05 communication with Arduino). if you have any answer to communicate with STM32WB5MMG Bluetooth module without any firmware development or if you have any example code to upload...
I have been trying to have the STM32WB55 save the OpenThread network information after joining the network, so that it can automatically join it upon power cycle. After joining the network through the commissioning process, I call SHCI_C2_FLASH_Store...
Is there any way to erase 32bytes in flash?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.