NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello all,I am working with the STM32WB series and using a 32 MHz crystal for the HSE (specifically the Murata XRCGB32M000F1SBBR0 on my custom board).To verify correct operation, I measured the analog waveform on OSC_IN and OSC_OUT using a low-capaci...
I'm working with a NUCLEO-STM32WBA55 board and trying to build the BLE_p2pClient example project, but it fails with the error shown below:I../../System/Modules -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -...
HelloI was developing an application that uses BLE and low power mode. I was testing that on a custom board and when I measured the current consumption at STOP2_MODE, it was 1.7 mA.I expected that I had made a mistake. So I tried the low power exampl...
Hi, I am using STM32WBA55G-DK1, is it possible to use Audio In jack to send the input audio and at Out to receive the audio in a full duplex method. Thank you
Hi Community, I'm trying to build the BLE_TransparentMode example for the NUCLEO-WB05KZ, but I'm getting the following build error: region 'FLASH' overflowed by 93348 bytes Steps to reproduce: Open the BLE_TransparentMode example from the MX Examp...
Hi!In AN5289, on page 37, the sequence for writing to Flash memory is described, taking into account potential CPU2 access (semaphores Sem2, Sem6, and Sem7). What does the diagram for writing/reading option bytes look like? Is it the same?
I am using the stm32wb55rev6 for my ble project.I created a new project based on the custom template provided by the ST. I am not able to print the messages on the terminal using the APP_DEBUG function.I am not able to send the data from the app to t...
Hi! We are developing a sensitive device using the STM32WB55, using in the M0+ the concurrent Thread+Ble binary (we use the concurrent because we'll need both Ble and Thread in the near future, althought the most important role is the Thread communic...
Use example code BLE_Audio_HAP_Central to audio function. The Central may start the stream fail, though the BLE connect and GAP link returns are OK. and Once the stream start failed, the stream cannot be start forever, with the result "CAP Unicast St...
Hi,I have couple of questions regarding the LORA Tx numbers specified in the ds for the stm32wle5.we are using VDD=3.3V , 22 dBm , ~928 Mhz LORA. 32 Mhz TCXOwe are NOT using the SMPS . table 29 in the ds mentions that typical current for...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.