2025-09-05 6:05 PM
Hello
I was developing an application that uses BLE and low power mode. I was testing that on a custom board and when I measured the current consumption at STOP2_MODE, it was 1.7 mA.
I expected that I had made a mistake. So I tried the low power examples found there STM32CubeWB/Projects/P-NUCLEO-WB55.Nucleo/Examples/PWR at master · STMicroelectronics/STM32CubeWB on my board and then using the P-Nucleo-WB55 and I found the current consumption is above 4 mA.
Shouldn't be measured in micro-ampere? I am confused now, as I am using an ST example and a dev board, so it should work well.
Thanks in advance.
Best regards,
Mahmoud A.
Solved! Go to Solution.
2025-09-16 5:21 AM
Hello,
before measurement with NucleoWB55 please remove everything from JP5 and JP2, also remove USB cable from ST-Link during measurement.
Please let me know if you can reach the stop mode current, thanks.
Best regards,
Filip Kremen
2025-09-12 6:12 AM
?
2025-09-16 5:21 AM
Hello,
before measurement with NucleoWB55 please remove everything from JP5 and JP2, also remove USB cable from ST-Link during measurement.
Please let me know if you can reach the stop mode current, thanks.
Best regards,
Filip Kremen
2025-12-01 9:51 PM
Hello @FilipKremen,
Yes, it solved the problem.
Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.