STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! 2.4Ghz Comms Example?

Hi.,Could anybody point me to a working example of a working basic IEEE  802.15.4 communication example, NOT Bluetooth, pure radio frequency in 2.4Ghz.I spent about 2 months trying to figure this out for my WB55 series without success and can't waste...

SteveJ by Associate II
  • 552 Views
  • 2 replies
  • 1 kudos

Resolved! How to get LTK

Hello community, I am currently considering capturing and analyzing BLE packets by using BLE sniffer, but for that I need the LTK used for decryption.BLE Secure Connection pairing does not directly exchange LTK, so I do not know where to find it exac...

Documentation Error re UARTs on B-WL5M-SUBG1 schematic

There appears to be mislabeling of PINs PC0 and PC1 on the MB1779B schematic pack. found  here  on sheet 3 of 8.  The PC0 and PC1 pins are mislabeled as UART1s but according to the datasheet for STM32WL5MOC they are actually LPUART1 as Alternate AF8....

PLaid.1 by Associate II
  • 447 Views
  • 1 replies
  • 1 kudos

Resolved! Question about WB55 Nucleo ADC example

I'm trying to implement the ADC to get V_BAT. I've done the set up in CubeMX in the IDE.I then went to the examples to see how a single ADC reading was done. I'm confused about the use of the following variables... /* Variables for ADC conversion dat...

STM32WBA55G-DK1 audio transmission Query

Hello, I have a query that can we send or stream the audio instead of Linein or Audio Jack, can we send it through CN12 or CN11 pins (UARTor SPI) from external UAC supported device in I2S format? If yes, could you please help me to configure it. I am...

Sandeep_k by Associate III
  • 408 Views
  • 0 replies
  • 0 kudos

Unable to get Core ID, No STM Target Errors

Hey there I have seen a few posts on this and tried a number of things:1 I went through the process in the user manual and get the error shown2. I tried to reboot board with the jumper moved to boot mode. I put it into UART mode but then got similar ...

Screenshot 2025-11-25 121648.png
RAdam.1 by Associate III
  • 707 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.