STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB55MMG BOOT0 and SW

In the datasheet of STM32WB5MMG, BOOT0 does not need to connect pull-up resistors and pull-down resistors, just connect GND or VCC directly.​In STM32WB5MM DK schematic,Do swdio and swclk need to be connected with pull-up or pull-down resistors? I wan...

_legacyfs_online_stmicro_images_0693W00000biv0xQAA.png _legacyfs_online_stmicro_images_0693W00000biurnQAA.png
Lep by Senior
  • 1437 Views
  • 0 replies
  • 0 kudos

What mode can I put my mcu in to consume the least amount of power but still have the ability to "wake up" after an event has been triggered?

I have a stm32 mcu. I want to put it in a very low power mode until an event triggers it to wake up. What mode can give me the lowest power consumption? whilst still being able to accept an event to wake up? and what sort of power would that draw?

LConn.2 by Associate
  • 1992 Views
  • 4 replies
  • 0 kudos

Unable to flash wireless stack to nucleo WB55RG

I am trying to do some testing with the new Matter protocol and using Thread and BLE on the Nucleo STM32WB55RG. Installing the new wireless stack firmware (found on the STM32 GitHub Hotspot), went just fine. After using the nucleo for a different use...

TStro.2 by Associate II
  • 2855 Views
  • 5 replies
  • 0 kudos

Enabling/Disabling Interrupts Problem in STM32WB55RG

Hello, I want to develop a software which includes an external interrupt for sleep mode and it should be enabled before entering sleep mode. For this purpose, I use: HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0) ;HAL_NVIC_EnableIRQ(EXTI0_IRQn); When I choos...

0693W00000aJCluQAG.png
Yusuf by Associate III
  • 3561 Views
  • 5 replies
  • 0 kudos

How to achieve low power Bluetooth advertising with STM32WB

I'm having issues getting the low power sleep to work with Bluetooth enabled on the STM32WBIs there any guide or app note on steps needed to achieve lowest power level BLE advertising?Basically no matter what I do - if I enable bluetooth advertising ...

ChrisLB by Associate III
  • 11503 Views
  • 16 replies
  • 2 kudos

Resolved! STM32WB5X BLE packets sizes

HiI would like to use STM32WB5MMG-DK.1) I tried to program 1.15 software packages for stack-ble + FUS + SAFEBOOT.The stack ble file size is 149KB, according to the release note it suppose to be programmed at address 0x080C5000 (or 0x080CE000).The FUS...

Ofer by Senior
  • 8532 Views
  • 5 replies
  • 0 kudos

Resolved! power consumption in stop modes,standby and shutdown mode

i am trying to measure the power consumption of the MCU in my custom board with different sleep modes, while measuring the stop2 mode i am getting consumption of 110 uA in the datasheet its showing of 2 uA ,even for shutdown and standby mode also its...

sabari1 by Associate III
  • 4163 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.