STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55RG BLE advertising issue

I am using nucleo STM32WB55RG to build an BLE application. I am having a very weird issue.At first I create an BLE application using CubeMX.I used server profile with custom template enabled (You can refer to attached cubemx file .ioc)The application...

PHoan.2 by Associate
  • 2530 Views
  • 4 replies
  • 3 kudos

STM32WL Memory definition in Lorawan_end_node

Hello,I am developing my own project based on Lorawan_end_node project, i have some doubts regarding to memory addressing. In linker file:/* Memories definition */ MEMORY { RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K NVM_RAM (rw) : ORIGI...

RPaja.1 by Associate II
  • 1393 Views
  • 1 replies
  • 0 kudos

STM32WLEx: Generated Binary file size is too large

Before release of package v1.3.0 binary size were <90kb and .ld has 3 partition in memory as below,/* Memories definition */MEMORY{ ROM  (rx)  : ORIGIN = 0x08000000, LENGTH = 256K RAM1  (xrw)  : ORIGIN = 0x20000000, LENGTH = 32K  /* Non-backup SRAM1 ...

PG26 by Associate II
  • 2719 Views
  • 3 replies
  • 0 kudos

Resolved! Flashing stm32wb5x_BLE_Stack_full_fw.bin start address

Hello. I am following document:https://github.com/STMicroelectronics/STM32CubeWB/blob/master/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/Release_Notes.htmlon how to flash STM32WB firmwares.I am going through steps:How to flash the Wireless Cop...

_legacyfs_online_stmicro_images_0693W00000biwPjQAI.png _legacyfs_online_stmicro_images_0693W00000biwXxQAI.png _legacyfs_online_stmicro_images_0693W00000biwmEQAQ.png _legacyfs_online_stmicro_images_0693W00000biwekQAA.png
LPetr.1 by Senior II
  • 8659 Views
  • 9 replies
  • 0 kudos

In STM32 using USB1 as an interface, when I flash the FUS version and BLE stack for the first time it is able to flash, but when I repeat the same steps then am not able to read the FUS version. Can anyone help me with this issue?

The steps performed:First read the FUS version.Selected the FUS bin file to flash.Flashed the above-mentioned file.Then again when I read the FUS version it was displaying as 00000000 in GUI

Mkuma.7 by Associate III
  • 6172 Views
  • 18 replies
  • 0 kudos

STM32wb15 is not advertising

I have 20 prototype custom boards, using STM32WB15CCU6E.Some of them advertise, some no (about 50%).If I program HeartRate binary, all advertise.Based on a clean project, I just added 1 service with 2 characteristics.Stack 1.15.0The log generated by ...

rbenv.3 by Associate II
  • 2999 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.