2023-04-24 2:22 AM
I have a characteristic1 as a write and I want to add a second characteristic as a read, but when I add this second I can't fint the device with the App?
Solved! Go to Solution.
2023-04-26 9:38 AM
Hello,
When you add a characteristic to a service, you should increase the value Max_Attribute_Records parameter when you call aci_gatt_add_service function.
The number of attribute records goes from 2 to 5 depending on the characteristic properties:
Best Regards
2023-04-26 9:38 AM
Hello,
When you add a characteristic to a service, you should increase the value Max_Attribute_Records parameter when you call aci_gatt_add_service function.
The number of attribute records goes from 2 to 5 depending on the characteristic properties:
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.