STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 User Manual RCC register is missing bit 18????

I am trying to incorporate the X-Cube-EEPROM package into an existing STM32WB55 Nucleo design that I have. In the process one of the compile errors refers to an RCC bit:​'RCC_CR_HSEBYP' undeclared (first use in this function); did you mean 'RCC_BDCR...

SWenn.1 by Senior III
  • 1237 Views
  • 2 replies
  • 0 kudos

STM32 LoRa Software Expansion for SX1261MB2xAS

I am looking for a suitable software package for the use of the SX1261MB2xAS shield with a NUCLEO platform.I already worked on a similar project some years ago and I am sure that I found and used an example for using this board in STM32CubeMX or STM3...

MWält.2 by Associate II
  • 2222 Views
  • 3 replies
  • 0 kudos

Resolved! Programming a Nucleo-WBA52CG

I was able to program two Nucleo-WBA52CG using STM32CubeIDE and the on board ST-Link. I programmed them with the BLE_HeartRateThreadX example application. When I power them I can see the BLE_HeartRateThreadX BLE traffic on my phone. However, I can no...

RCool.1 by Associate II
  • 1916 Views
  • 1 replies
  • 1 kudos

Issue with STM32CubeIDE - Import STM32Cube Example. After importing it compiles, when doing simple HW change in CubeMX there are many compilation errors.

Here is what I try to do:Imported SubGHz_Phy_PingPong to my workspace.Double click on IOC to launch CubeMX and do simple HW change, in my case enabling EXTIO interruptsAfter code generation there are many compilation errorsCan be reproduced with othe...

_JUhri.1 by Associate II
  • 7176 Views
  • 19 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.