NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have a burst sampling MCU application that wakes up via interrupt, samples, and should now signal a backend through LoRaWANThe CubeMX skeleton spins up a whole system with sequencer, power mode management etc, which is - did I get this right? - bu...
I am confused because I thought I have read somewhere that on the STM32WL55JC, only the M0+ Core is connected to the RF part and therefore M4 core normally hosts app code, M0+ core the RF part.In the examples I have seen for the Nucleo WL55JC there a...
On a custom board, the RED_LED is connected to PA15, which is pulled-up by default (JTDI).The pin has been set to Push-Pull Output GPIO in CubeMX and is initialized to 0.The STM32WB55CGUx was experiencing random resets, until this particular IO was s...
Attached is the IOC setup for simple continuous PWM Mode from LPTIM1 from STM32BW55 (all Cube IDE/MX updated with the library, etc).. RB2 showing the waveform as per Peroid and Pulse width (from 64MHz clock input) but I get no interrupt (enabled by I...
HiI need to know that how can i create thousand amount of binary or hex file for different keys during mass production. I use custom firmaware, sdk v.1.0 for development and i wrote manually keys of each device.
Hi, I need some help trying to undestand this operation in Lorawan_end_node example projectnvm_size = ( ( sizeof( LoRaMacNvmData_t ) + 7 ) & ~0x07 ); in the code below:Maybe it is so simple, but i thought that it would be something like that nvm_siz...
Hello everyone:I created a thread udp project through the official Max 6.7 version of the IDE and applied it to two Nucleo -STM32WB55 development boards for thread data transmission.(One as FTD equipment, one as MTD equipment)I want to let the MTD...
Hey!!I have a BLE application which runs on custom server profile. There are few characteristics of a given service, where the client can modify them. I need clarifications for the below questions.Is there any event generated by the BLE stack to know...
Hello ST,I am using STM32WB Necleo Board to test USB as VCP. my reference project is BLE_MeshLightingLPN (USB Dongle) project and same way i am implementing all libraries and modification in BLE_MeshProvsion... CFG_USB_INTERFACE_ENABLE 1A new VCP por...
Looking at the website it cost a lot of money , approx $5k .https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/qualification-listing-fees/Scott
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.