2023-04-30 1:15 PM
I am looking for a suitable software package for the use of the SX1261MB2xAS shield with a NUCLEO platform.
I already worked on a similar project some years ago and I am sure that I found and used an example for using this board in STM32CubeMX or STM32CubeIDE.
Now I can only find the I-CUBE-LRWAN package which is suitable for another hardware platform.
2023-04-30 3:26 PM
Which STM32?
The LRWAN package can be ported to other plaforms, the most common used would be L0 and L4
Are you looking to do LoRa PTP or LoRaWAN?
2023-04-30 11:26 PM
The platform doesn't really matter to me.
It will probably be F4/G4/L4. For the first tests, we want to use the existing NUCLEO-F446RE.
The focus will be on LoRaWAN.
The most obvious project I have found for this is the
following:
en.i-cube_lrwan\STM32CubeExpansion_LRWAN_V2.1.0\Projects\NUCLEO-L476RG\Applications\LoRaWAN\LoRaWAN_End_Node\STM32CubeIDE\sx1261dvk1bas
However, porting this project seems to me to be relatively costly. However, I may be missing something in the process.
I would start by cleaning up the application of any extra components on the dev board, such as LCD.
Then I would adapt the NUCLEO specific parts for my platform.
Finally, our application should upload a few sensor values cyclically and get configs for the sensors if needed.
2023-04-30 11:29 PM
Since we don't have the dev board for which I found an example project. We can never check during the modification of the program whether everything "still" works.
Therefore I am looking for a less extensive End Node sample
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.