2023-05-03 6:30 AM
Hi
We develop a project on the STM32WB5MMG MCU. We have 2 issues:
1. How can we get the actual MTU after the negotiation with the remote client (probably a smartphone) ? We want to support all kind of smartphones including those with small MTU. Do we have to be worried about this issue in case of transmitting too large packets to the client or would the packet be divided into sub-packets automatically ?
2. When working with the debugger on both EVB (STM32WB5MMG-DK) and our board is ok, both after disconnecting power and connecting it again, we don't get advertise again. Have someone now what cause this ?
Thanks
2023-05-03 9:35 AM
Hello,
Best Regards
2023-05-03 11:48 AM
Dear Remy
Thanks for your reply.
2023-05-04 12:31 AM
Hello,
I think you are facing a known issue, can you open your linker file (STM32WB5MMGHX_FLASH.ld) and check if you have an extra dot for MB_MEM2 section (e.g *(.MB_MEM2) ; instead of *(MB_MEM2) ;) ?
If yes, remove the extra dot and it will work. Due to this extra dot, the buffers that need to be in SRAM2 are not placed there, so your application doesn't work. It will be corrected in the next release of STM32CubeIDE tool.
Best Regards
2023-05-08 5:26 AM
Dear Remy
It seems that there is only option to set this parameter, how can I get it ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.