2023-05-09 4:10 PM
Hi all !
Does anyone know if it's possible to port SPI Emulator to the STM32WB5MMG family ? (or have an example of a possible implementation from scratch ?)
I would like to implement a simple slow half-duplex master SPI protocol using custom ports.
Did give a quick try to adapt the existing library for STM32F but for the moment the compilator mainly complains about this portion of the code (tried to create stm32wbxx_hal_def similarly to what's existing for STM32F series because it doesn't exist in hal library but spi emul needs it)
#define __HAL_LINKDMA(__HANDLE__, __PPP_DMA_FIELD__, __DMA_HANDLE__) \
do{ \
(__HANDLE__)->__PPP_DMA_FIELD__ = &(__DMA_HANDLE__); \
(__DMA_HANDLE__).Parent = (__HANDLE__); \
} while(0)
with error "request for member "hdma" in something not a structure or union."
And this is where I'm starting to believe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.