NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello All,I'm starting a project based on a STM32WL.After downloading the "SubGHz_Phy_Per" project I try to duplicate the project for my custom board based on the STM32WLE5CBUX.The "SubGHz_Phy_Per" project provide the HAL_Delay(Delay) via a call to t...
Good Morning,I’m a little bit lost with your REACH certificate. Can you tell me which category the products below belong to ?LIS2DH12TR MLPF-WB55-01E3 STM32WB30CEU5A Are there SVHC in this products ? Thanks
Hi,I am creating a battery operated device using the STM32WB10 and I need to figure out how to make use of the claimed 30nA shutdown current consumption. (I realize this is at certain voltage and temperature ranges).The best I have been able to achie...
Hi,I would like to refer to the P-NUCLEO-WB55 example BLE_Custom and apply it to the stm32wb30 custom board.I have succeeded in operating BLE_Custom in LPM mode on NUCLEO-WB55 by referring to the following questions.Stm32WB custom BLE example issue w...
Via USB interface the -rst using CLI was not working and even in GUI these options were grayed out or not available. Please refer the below images for reference.Using the WB package - 1.15Using the STM32Cubeprogrammer - 2.12Is there any possible way ...
we are strugling in our project that is now in a trial with the customer and I need your tech support to provide the information on the way to increase the TX power to maximum. We are now seeing a -30dbm directly from the STM32WLE5JCI6 pinout RFO_HP...
Hello,I'm currently working on an application that integrates the LoRaWAN stack (version 2.1.0), and has to use USART2 to send/receive data. USART2 is already used by the trace utility, to send trace messages. I activated RX on interruption by callin...
We are working with android and there are multiple problems it is causing us with its Service Changed characteristic.Is there a way it will not be created? Some chcekbox in CubeMx or else?Cheers!
Hi,We are designing ou custom Lora application based on the STM32WLE5CCU6 MCU.1- We would like to know if there is an eval board that can be used in manufacturing tests to perform a pingpong communication test (between our custom board and the eval b...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.