2023-04-10 2:47 AM - edited 2023-11-20 8:35 AM
Via USB interface the -rst using CLI was not working and even in GUI these options were grayed out or not available. Please refer the below images for reference.Using the WB package - 1.15
Using the STM32Cubeprogrammer - 2.12
Is there any possible way to reset the microcontroller via USB?
2023-04-19 4:37 AM
Hello @Mkuma.7,
Thanks for your feedback,
The reset via USB is only available for MPUs, the screenshot you shared is from the Available commands for STM32 MPU section of the help menu. For MCUs, this instruction is only available via ST-LINK interfaces.
Aziz
2023-04-19 6:15 AM
Hello Aziz BRIGUI,
So you mean there is no way to reset the micro-controller, right?
2023-04-19 6:16 AM
I mean via USB
2023-04-24 3:13 AM
Hello @Mkuma.7,
Yes, as far as I know, there's no way to reset the MCU via USB with STM32CubeProgrammer.
Aziz
2023-06-05 4:34 AM
Hello Aziz,
Is there any way via FUSES to reset the micro-controller?
2023-06-13 2:11 AM
@Aziz BRIGUI
Is there any way via FUSES to reset the micro-controller?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.