STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

CMSIS_V1 problem

I am using a "STM32WB55 Nucleo Pack", when I trie to active the FREERTOS in a new project i can't choose the CMSIS_V1 interface and I need it to use the M0 and M3 processors.Instead of this, i can choose the CMSIS_V2, but I need the CMSIS_V1.Could an...

JSanc.7 by Associate II
  • 844 Views
  • 0 replies
  • 0 kudos

BLE Tx power PA_Level vs Min Max

what is the relation between shci function input struct :  SHCI_C2_Ble_Init_Cmd_Param_t/** Minimum transmit power in dBm supported by the Controller.* Range: -127 .. 20*/int8_t min_tx_power;/*** Maximum transmit power in dBm supported by the Controll...

DS.4 by Senior II
  • 2136 Views
  • 0 replies
  • 0 kudos

STM32WB55, write in the internal flash memory with FreeRTOS

Hi, I try to save the configuration application in the internal flash memory of my STM32WB55 with this next fonction : static int write(long offset, const uint8_t *buf, size_t size) { size_t i;   uint32_t addr = stm32wb_onchip_flash.addr + of...

RJARC.1 by Associate II
  • 2149 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLxx possible wrong sync word register address

Hi, i had a problem when i try to implement a bare metal code for STM32WLE5JC for GFSK modulation. The sync word in the reference manual of the MCU state that begin from registers SUBGHZ_GSYNCR0 - SUBGHZ_GSYNCR7 (Addresses:0x06C7 - 0x06C0), so it can...

XKeto.1 by Associate
  • 1396 Views
  • 3 replies
  • 0 kudos

STM32WLE5CCU6 / EU433 Requirement

Hi, Our custom module, built around the STM STM32WLE5CCU6 chipset, has been designed accordingly. However, we have received a new requirement from the customer regarding the EU433 region frequency. Could you please provide us with the application not...

Stm32wb10ccu5 ble not working in costom bord.

Im using stm32wb10ccu5 in my pcb i check everything possible. Try all resources in get. Try a lots of programs. But my devices not creating any Bluetooth zone. Now I am so fed up that I decide to move on ESP32. But before that I came here to  express...

SMazu.3 by Associate III
  • 766 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.