2023-06-16 9:46 AM
Hello All,
I'm starting a project based on a STM32WL.
After downloading the "SubGHz_Phy_Per" project I try to duplicate the project for my custom board based on the STM32WLE5CBUX.
The "SubGHz_Phy_Per" project provide the HAL_Delay(Delay) via a call to the TIMER_IF_DelayMs(Delay) defined in the timer_if.c . And it works. The code is clear.
void TIMER_IF_DelayMs(uint32_t delay)
{
/* USER CODE BEGIN TIMER_IF_DelayMs */
/* USER CODE END TIMER_IF_DelayMs */
uint32_t delayTicks = TIMER_IF_Convert_ms2Tick(delay);
uint32_t timeout = GetTimerTicks();
/* Wait delay ms */
while (((GetTimerTicks() - timeout)) < delayTicks)
{
__NOP();
}
/* USER CODE BEGIN TIMER_IF_DelayMs_Last */
/* USER CODE END TIMER_IF_DelayMs_Last */
}My project provide the HAL_Delay(Delay) via a call to the TIMER_IF_DelayMs(Delay) defined in the timer_if.c
But the code is not the same and the HAL_Delay return without wating any delay.
void TIMER_IF_DelayMs(uint32_t delay)
{
/* USER CODE BEGIN TIMER_IF_DelayMs */
/* USER CODE END TIMER_IF_DelayMs */
}I cannot find where I can configure the project to duplicate the configuration of the "SubGHz_Phy_Per" project.
I already try to change the "System Core / SYS / Timebase Source" between None and SysTick but it didn't change anything.
Could you help me ?
Best Regards
Matthieu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.