NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I'm working with stm32wb5mmgh to transmit data. The thing is BLE starts to advertise only in the debug mode if I upload it in the device its not showing. So what I did I turned on led when it starts to advertise as I mentioned in the below code. ...
Hi Team, I am searching for STM32WBA52CGU6 circuit diagram unfortunately not able to found out because the file was not found in our ST website. Kindly help me to get the exact circuit for my project purpose.
Hi All,I'm using STM32WL55JC board which include Sub-GHz, ADC and DMA peripherals (and many more of course)I run "ping pong" example to create Sub-GHz communication sucssfully, also run "ADC_SingleConversion_TriggerTimer_DMA" and changed to circular ...
My project need to synchronize the clock of our STM32WL device with TTN server. How can I use the function in LmhpClockSync.c to do the job ? I would be grateful if any expert can guide me to get it done.
Hello,I use B-L072Z-LRWAN1 and I would like to know how to use it in very low power consumption. By default on mbed OS 6 with one hand with only one ThisThread::sleep_for(3s) I have a consumption of 10.45mA. I take my measurements with an amperemeter...
I'm using a STM32WLE5 processor in my design. I had an RF consultant tell me that I needed to add a SAW filter to the design to protect against potential interference with 800 MHz cell phone transmissions so I placed a B39921B3728U410 SAW filter at t...
Hi Team,Can I use this IPD Filter 0900FM15D0039E in the instead of the passives in the design fof STM32WLE5 MCU for RF (915 MHz).
Hellofriends, I am trying to make a dual core example on the Wio-E5 STM32WLE5JC Module. I made all the settings as in this video. However, only CM4 works when debugging. CM0PLUS is not working and I am getting this error Target unknown error 32Error...
Hi,I have been trying to launch on a Nucleo WB55 board some default apps available in STM32CubeWB-1.14.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE with the latest version of the BLE_stack_full_extended. (e.g. BLE_HealthThermometer, BLE_Ota)But t...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.