NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, For a personal project, I am designing a device that receives GPS data and transmits the UTC time information to other devices over BLE. I will also be designing a device that receives the data and displays it. For this, I have chosen the STM3...
I've been working with the STM32WB55 microcontroller and have been trying to set up 4 bit trace functionality (ETM, not SWO) for debugging. I've connected the trace pins according to the datasheet and configured them in the STM32Cube software.Specifi...
I'd like to know if it is possible to cascade two LPTIM in order to make a 32-bit counter. I'm implementing my main LoRa application with the sequencer but I need to have 32-bit hardware counter running continously in the background to count external...
I've modified basic HeartRate project to run an ADC inside of the task. However this results in adc always returning 0. Sometimes whole application hangs. However when CFG_LPM_SUPPORTED is set to 0. Everything works fine. I've already created github...
Hello,I am working on a STM32WB55RG BLE Project and the problem is that about once in every 3 program that I upload, BLE doesn't work. After reupdating the BLE Stack firmware, it works correctly. I am using the BLE firmware v1.16.0.4. What could be ...
Hi,I'm working on STM32WL55JC board and run "TIM_PWMOutput" example that run 4 PWM channels with diffrence pulse width.I'm trying to add deadtime between the channels (following this hands-on video https://www.youtube.com/watch?v=rDaC2N-33Oo Minute ...
I modified the LoRaWAN_End_Node sample program for measuring the external pulses input to the COMP1. I register a task in the sequencer and set up the timer in timer server. It is no problem to run a test task by just toggle the LED. When I initializ...
Hi Sirs, I've fiddled around Cable Replacement Example code (CRS for server). I successfully created a custom function to send a char string to the peripheral upon pushing SW1. Now my problem is when I made a new project, with an .oic file, created ...
Hello AllI have a cutom board. I am working on STM32WB55VGQ6(BGA129).2 crystals(32.768KHz, 38MHz) output waves are not coming.I checked waveform by using an oscilloscope and OSC-IN/OUT pins are ground level(0V)Voltage conditions all 3.3V : VDD, VDDUS...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.