2022-07-20 3:31 AM
Hi,
I have been trying to launch on a Nucleo WB55 board some default apps available in STM32CubeWB-1.14.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE with the latest version of the BLE_stack_full_extended. (e.g. BLE_HealthThermometer, BLE_Ota)
But then the BLE seems to crash at startup and doesn't even advertise.
If I just replace the co-proc image with the "_full" one instead of "_full_extended", then the example app is working fine.
Any explanation on such a limitation?
Thank you,
Best regards.
2022-07-21 6:19 AM
Hello,
In order to use the BLE Full stack extended, it is necessary to adapt the scatter file in the BLE applications.
If you want to use extended feature, two examples are available in STM32CubeWB package: BLE_p2pServer_Ext and BLE_p2pClient_Ext.
A wiki page about Wireless Stack will be available soon.
Best Regards
2023-07-13 10:30 PM - edited 2023-07-13 10:31 PM
Hi, I had the same problem. Just replace linker file STM32WB55RGVX_FLASH.ld from the BLE_p2pServer_Ext example. Don't forget to clean your project before.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.