2023-07-13 10:12 AM
Hello
friends, I am trying to make a dual core example on the Wio-E5 STM32WLE5JC Module. I made all the settings as in this video. However, only CM4 works when debugging. CM0PLUS is not working and I am getting this error Target unknown error 32
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target. I tried this on STM32Cube ide 1.7.0 and 1.8.0.
Solved! Go to Solution.
2023-07-14 1:28 AM - edited 2023-07-14 1:40 AM
Hello @FAlpa.1 and welcome to ST Community .
Wio-E5 is based on the STM32WLE5JC wish use just a single core ( Cortex-M4 ). you can't use it with a dual core application. I suggest you try an STM32WL5XXX for a dual core application.
I hope this is helpful.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-14 1:28 AM - edited 2023-07-14 1:40 AM
Hello @FAlpa.1 and welcome to ST Community .
Wio-E5 is based on the STM32WLE5JC wish use just a single core ( Cortex-M4 ). you can't use it with a dual core application. I suggest you try an STM32WL5XXX for a dual core application.
I hope this is helpful.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.