2023-07-05 12:40 AM - last edited on 2023-07-07 6:59 AM by Amel NASRI
Hi,
I'm working with stm32wb5mmgh to transmit data. The thing is BLE starts to advertise only in the debug mode if I upload it in the device its not showing. So what I did I turned on led when it starts to advertise as I mentioned in the below code.
/* Update Advertising data */
ret = aci_gap_update_adv_data(sizeof(a_AdvData), (uint8_t*) a_AdvData);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("==>> Start Fast Advertising Failed , result: %d \n\r", ret);
}
else
{
APP_DBG_MSG("==>> Success: Start Fast Advertising \n\r");
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);
}
The LED turned on after I uploaded the code but the BLE is not showing.
Used FUS Version : v1.2.0.0, STACK Version : v1.16.0.4, stm32wb5x_BLE_Stack_full_fw.bin.
Also I change the linker Script as mentioned in this wiki link. I also share the linker script.
/*
******************************************************************************
**
** File : LinkerScript.ld
**
** Author : STM32CubeIDE
**
** Abstract : Linker script for STM32WB5MMG Device
** 1024Kbytes FLASH
** 256Kbytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is without any warranty
** of any kind.
**
*****************************************************************************
** @attention
**
** Copyright (c) 2022 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
*****************************************************************************
*/
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM1) + LENGTH(RAM1); /* end of RAM1 */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 512K
RAM1 (xrw) : ORIGIN = 0x20000008, LENGTH = 0x2FFF8
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 2K
RAMB_SHARED (xrw) : ORIGIN = 0x20038000, LENGTH = 10K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* The program code and other data goes into FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data goes into FLASH */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
.ARM : {
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} >FLASH
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} >FLASH
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} >FLASH
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} >FLASH
/* used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM1 AT> FLASH
/* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM1
/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM1
/* Remove information from the standard libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
MAPPING_TABLE (NOLOAD) : { *(MAPPING_TABLE) } >RAM_SHARED
MB_MEM1 (NOLOAD) : { *(MB_MEM1) } >RAMB_SHARED
/* used by the startup to initialize .MB_MEM2 data */
_siMB_MEM2 = LOADADDR(.MB_MEM2);
.MB_MEM2 :
{
_sMB_MEM2 = . ;
*(.MB_MEM2) ;
_eMB_MEM2 = . ;
} >RAMB_SHARED AT> FLASH
}
can any one help me with this issue??!!
2023-07-12 2:06 PM
Hello @LR.2 ,
There has been a case created to resolve this question and we will be reaching out to you directly.
Regards,
Roger
2023-07-16 10:42 PM
Hey Roger,
Thanks for your timely response. I hope to hear from you soon.
Regards,
Lakshmanan
2023-07-19 3:16 AM
Hello,
The modification around the linker script describes in the wiki pages need to be done when using extended binaries (stm32wbxx_BLE_Stack_full_extended_fw.bin, stm32wbxx_BLE_HCILayer_extended_fw.bin), in your case it's not needed. You are currently facing to this issue:
https://community.st.com/t5/wireless-mcu/pay-attention-issue-in-stm32cubeide-linker-template-file-causes/m-p/55840
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.