2023-07-14 4:41 AM
Hello,
I am working on a STM32WB55RG BLE Project and the problem is that about once in every 3 program that I upload, BLE doesn't work. After reupdating the BLE Stack firmware, it works correctly. I am using the BLE firmware v1.16.0.4. What could be the problem?
Best Regards,
Yusuf
Solved! Go to Solution.
2023-07-21 6:37 AM
Hello, I used STM32-USB-VCOM example shared by STM on custom board. However, I seen the same problem using P-Nucleo-WB55 dongle with Heart Rate example. I used the fix you have shared in Solved: STOP2 low power on STM32WB55 with BLE connection w... - STMicroelectronics Community and now it seems fixed for now but I will continue to check it.
Best Regards,
2023-07-20 9:28 AM
Hello,
Can you give more details on your issue? Are you using application form STM32CubeWB package or you have create your application ? Are you working on nucleo board or on custome hardware ?
Best Regards
2023-07-21 6:37 AM
Hello, I used STM32-USB-VCOM example shared by STM on custom board. However, I seen the same problem using P-Nucleo-WB55 dongle with Heart Rate example. I used the fix you have shared in Solved: STOP2 low power on STM32WB55 with BLE connection w... - STMicroelectronics Community and now it seems fixed for now but I will continue to check it.
Best Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.