2023-07-19 9:17 PM
Hi Sirs,
I've fiddled around Cable Replacement Example code (CRS for server). I successfully created a custom function to send a char string to the peripheral upon pushing SW1. Now my problem is when I made a new project, with an .oic file, created a custom service with read and write characteristics (write specifically my concern), then ported my custom function.
When I debug my code, I was able to call the event by pressing the SW1, up to the code aci_gatt_update_char_value(), but nothing is showing on the terminal. Im sure this works on the Cable replacement code. I even copied the UUIDs of the service and characteristics of Cable replacement. but to no avail.
Here is the initialization of my write service
/**
* CharW01
*/
COPY_CHARW01_UUID(uuid.Char_UUID_128);
ret = aci_gatt_add_char(CustomContext.CustomMysvcHdle,
UUID_TYPE_128, &uuid,
SizeCharw01,
CHAR_PROP_READ | CHAR_PROP_WRITE_WITHOUT_RESP,
ATTR_PERMISSION_NONE,
GATT_NOTIFY_ATTRIBUTE_WRITE,
0x10,
CHAR_VALUE_LEN_VARIABLE,
&(CustomContext.CustomCharw01Hdle));
Here is the code for updating the characteristic (CHARW01)
tBleStatus Custom_STM_App_Update_Char(Custom_STM_Char_Opcode_t CharOpcode, uint8_t *pPayload)
{
tBleStatus ret = BLE_STATUS_INVALID_PARAMS;
uint8_t size;
size = 0;
while(pPayload[size] != '\0'){
size++;
}
switch (CharOpcode)
{
case CUSTOM_STM_CHARW01:
ret = aci_gatt_update_char_value(CustomContext.CustomMysvcHdle,
CustomContext.CustomCharw01Hdle,
0, /* charValOffset */
size, /* charValueLen */
(uint8_t *) pPayload);
break;
case CUSTOM_STM_CHARN02:
ret = aci_gatt_update_char_value(CustomContext.CustomMysvcHdle,
CustomContext.CustomCharn02Hdle,
0, /* charValOffset */
SizeCharn02, /* charValueLen */
(uint8_t *) pPayload);
break;
default:
break;
}
return ret;
}
When I use this code under cable replacement and then download it on nucleo device, I am able to send strings, but not on my project.
Have I missed something in porting this code on my new project? Im not quite sure if I need to follow some GATT coding in order for me to correctly replicate the cable replacement.
Thank you so much.
Ian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.